"+CMS ERROR: network timeout" on SMS send after 4-6 days

I’m near desperate to solve this.
I’m trying to replace SIM800L modules with SIM7670NA(or SIM7670G) before 2/3G fully stops on T-Mo.

So in months of testing SIM76XX modules(core boards), something happens after 4-6 days of being connected(on T-Mo). I have the APN set and the UART timeout of the SIM7670NA disabled. I have tried sending the AT command every 4 hours, 8 hours, with the same results. There is no CMS Error number given.

There is very little intel on the web about “+CMS ERROR: network timeout”. Once these show up, SMS message take 15-20 minutes to deliver to the module, and daily SMS auto-test messages fail to send, or are delayed hours. This was never problem using SIM800L modules, they just worked reliably. The modules I’m using are T-Mobile certified. mobile phones don’t seem to have this problem.

Should the module be power-cycled every couple days?
Any advice greatly appreciated.

Whats the part number of the kit/module you’re using? Who made it? I’m trying to look up documentation to read along.

Hi Kristof,
Sorry it’s not from DK.
See it here
Or this one.

We have been working with 4-5 different SIMCom boards, different suppliers, with same issue.

Your link to AliExpress had this customer review which I find concerning regarding the Seller’s Reply:

Have you tried reaching out to ANDTech? I’m finding their documentation on this module extremely limited.

We’re currently testing a SIM7670NA module in the first link (not AND). We have communicated with suppliers, (even the US sales rep for SimCom) more than a few times explaining that we were replacing SIM800L modules in agricultural systems using SMS and they have never mentioned SMS problems. Our tests seem to be doing MUCH better than the review you found. It sites horrible immediate errors unlike I have never seen. I will setup a SIM7670NA from AND Technologies and see if there is a difference. AND is very good to communicate with, and would probably help diagnose issues(to some extent). There are so many more factors involved with sending SMS with 4G LTE(modules), compared to 2G/3G, like APN, SMS service center address, PDP, etc. I’m definitely not an expert at this, but I understand the 4G modules are using packet data, not the (circuit-switched network) back-end as were the 2G devices.

I was feeling like the module needs to be reset or power-cycled on a regular basis, or requires a configuration I’m unaware of. I’ve never found a class, webinar, website, or a book about designing products using 4G LTE modules. While the manufacturers have little support.

Unfortunately this is not a product we sell at DigiKey. If there are performance issues the Manufacturer of the parts has to help. Otherwise the place that sold them. Right now companies are coming back from 2 weeks off for the holidays . This could explain the lack of communication. I would say you need to wait for their response. Others do watch the forum so maybe someone might be able to offer a solution.

I had a similar issue and found out the modem’s network registration was dropping after a few days. I fixed it by periodically checking and re-registering with the network in software.

I created a resend SMS on error loop and it seems to have solved the CMS send errors. I need to try the re-registration I guess because seems like because of the deprioritization, that I’m reading more and more about, regarding iot devices, that receiving SMS can sometimes be delayed (a half hour plus sometimes in our tests). This makes some of our products useless, where if a farmer needs to quickly turn something off, like grain flowing or a feeder, it can’t be done instantly every time. That’s bad.

That’s good information to share, thanks Sid! The timing issue is unfortunate and does need solving for these systems. If our team comes up with anything, I’ll be sure to drop it in here.

I ran into that with SIM7600s on T-Mo, they’d work fine for a few days then suddenly hang with long delays on SMS. Ended up adding a watchdog to force a reboot every 48h, and that kept things stable. Annoying but it worked. What’s weird is I tested bulk sms delivery during that time and messages reached phones instantly, so it really feels like the module just stops handling network sessions right.