Compatibility of a tool and part

Hi I was wondering if the tool DL-3460R could be used with any of the following parts
937-SP-301010R
SS-30100-019
32-5910UL

Thanks

937‑SP‑301010R and SS‑30100‑019 are supported by DL-3460R. Not sure about 32-5910UL.

Hello fhoutaham and welcome to the DigiKey TechForum,

DL-3460R would be intended to be used with these modular connectors, but it is possible that it could work with the ones you listed. They do match the type that the crimper has listed as “For Use With”.

937-SP-301010R and SS-30100-019 list the same field installation crimpers/die set:

Die set 2990008-01
Crimper 2990007-01

For 32-5910UL lists for use with crimper part number:

24-7865P