See attached pics. Need help locating this crimp connector. With and without wire leads.
Welcome to the technical forum. Can you provide more details? Can you provide the housing that this is installed in?
There seems to be two posts on the same subject. Did you check the resonse from Irfan ? WE would need the pitch which is the measurement from the center of one hole to the center of the next one. We would also need the wire gauge you are going to use.
Not using the plug. only crimped connector. Wire size is 22awg.
We need to be able to identify that housing before we find the Terminal that would be used in it.
Looks like you have 1-1123722-4 TE Connectivity AMP Connectors
Contact Part Number found here: 1318912-1
I do not see that we have a pre-terminated wire option for this.