I am trying to replace a 172mm DC fan that had 0-5VDC speed input.
Comair makes 2 fans that might work:
- 19039695A (Digikey CR588-ND) and
- 17001197A (Digikey CR626-ND)
My “problem” is the datasheets are not explicit about the analog speed input voltage range.
This Comair document says the analog voltage is “typically” 1/2 the rated voltage:
http://www.comairrotron.com/different-methods-control-fan-speed
In the “PROGRAMMABLE” section:
The rule of thumb is a zero voltage input will result in a minimum speed condition and an input equal to 50% of the fans nominal voltage will result in a maximum speed condition. For instance, a 24vdc fan will operate at full speed when 12vdc is applied to the program lead.
The data sheet for ONE fan says:
PWM Input, 5 volt TTL
Clearly suggesting it is a 0-5VDC input
The other says:
PWM: 200 ~ 2 KHz, Open Collector
No voltage specified, which is consistent with the “rule of thumb” of 1/2 rated voltage or 0-12VDC.
Is there any way to find out, exactly, what each of these fans will accept for speed input?
Thanks in advance,
Please CC replies to my tech: richard.cooke@gnv.ca