This is a page about Octavo Systems’s OSD62x-PM; https://octavosystems.com/octavo_products/osd62x-pm/
Availability
Boards:
- OSD62-PM-BRK at DigiKey
Serial Cable:
- Raspberry Pi Serial Probe at DigiKey
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- Kernel.org Cross Compilers – https://mirrors.edge.kernel.org/pub/tools/crosstool/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- arm64 based rootfs
- Debian: https://www.debian.org
Cross Compiler: 32bit arm-linux-gnueabi-gcc
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://mirrors.edge.kernel.org/pub/tools/crosstool/files/bin/x86_64/11.5.0/x86_64-gcc-11.5.0-nolibc-arm-linux-gnueabi.tar.xz
tar -xf x86_64-gcc-11.5.0-nolibc-arm-linux-gnueabi.tar.xz
export CC32=`pwd`/gcc-11.5.0-nolibc/arm-linux-gnueabi/bin/arm-linux-gnueabi-
Test Cross Compiler:
#user@localhost:~$
${CC32}gcc --version
#Test Output:
arm-linux-gnueabi-gcc (GCC) 11.5.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Cross Compiler: 64bit aarch64-linux-gcc
This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:
#user@localhost:~$
wget -c https://mirrors.edge.kernel.org/pub/tools/crosstool/files/bin/x86_64/11.5.0/x86_64-gcc-11.5.0-nolibc-aarch64-linux.tar.xz
tar -xf x86_64-gcc-11.5.0-nolibc-aarch64-linux.tar.xz
export CC64=`pwd`/gcc-11.5.0-nolibc/aarch64-linux/bin/aarch64-linux-
Test Cross Compiler:
#user@localhost:~$
${CC64}gcc --version
#Test Output:
aarch64-linux-gcc (GCC) 11.5.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Bootloader:
Pre install a few host packages with build-essential and git, which will be utized to build everything else.
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y build-essential git
Bootloader: TI Linux Firmware
The TI Firmwares are required for functionality of the system: https://git.ti.com/gitweb?p=processor-firmware/ti-linux-firmware.git;a=shortlog;h=refs/heads/ti-linux-firmware
Download:
#user@localhost:~$
git clone -b 10.01.10 https://github.com/beagleboard/ti-linux-firmware.git --depth=1
Bootloader: Trusted Firmware A
Trusted Firmware for A profile Arm CPUs: https://git.trustedfirmware.org/plugins/gitiles/TF-A/trusted-firmware-a.git/
Download:
#user@localhost:~$
git clone -b lts-v2.12.6 https://github.com/TrustedFirmware-A/trusted-firmware-a.git --depth=1
Build:
#user@localhost:~$
make -C ./trusted-firmware-a/ -j4 CROSS_COMPILE=${CC64} PLAT=k3 ARCH=aarch64 SPD=opteed TARGET_BOARD=lite all
Bootloader: OP TEE
Open Portable Trusted Execution Environment (OP-TEE): https://github.com/OP-TEE/optee_os
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y python3-cryptography python3-minimal ; \
sudo apt-get install -y python3-pyelftools
Download:
#user@localhost:~$
git clone -b 4.7.0 https://github.com/OP-TEE/optee_os.git --depth=1
Build:
#user@localhost:~$
make -C ./optee_os/ -j4 CROSS_COMPILE=${CC32} CROSS_COMPILE64=${CC64} CFG_ARM64_core=y PLATFORM=k3-am62x CFG_WITH_SOFTWARE_PRNG=y all
Bootloader: U-Boot
Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y bc bison flex libgnutls28-dev libssl-dev; \
sudo apt-get install -y python3-dev python3-jsonschema ; \
sudo apt-get install -y python3-setuptools python3-yaml ; \
sudo apt-get install -y swig uuid-dev yamllint
Download:
#user@localhost:~$
git clone -b v2024.04-ti-10.01.10-am625-osd625-brk https://github.com/RobertCNelson/ti-u-boot-octavo.git --depth=1
Configure and Build: Cortex-R5
#user@localhost:~$
make -C ./u-boot/ O=../CORTEXR CROSS_COMPILE=${CC32} am62x_osd62x_r5_defconfig ; \
make -C ./u-boot/ -j4 O=../CORTEXR CROSS_COMPILE=${CC32} BINMAN_INDIRS=../ti-linux-firmware/
Copy Build Objects: Cortex-R5
#user@localhost:~$
mkdir -p ./input/ ; \
cp -v ./CORTEXR/tiboot3-am62x-hs-fs-osd62x.bin ./input/
Configure and Build: Cortex-A53
#user@localhost:~$
make -C ./u-boot/ O=../CORTEXA CROSS_COMPILE=${CC64} am62x_osd62x_a53_defconfig ; \
make -C ./u-boot/ -j4 O=../CORTEXA CROSS_COMPILE=${CC64} BL31=../trusted-firmware-a/build/k3/lite/release/bl31.bin TEE=../optee_os/out/arm-plat-k3/core/tee-pager_v2.bin BINMAN_INDIRS=../ti-linux-firmware/
Copy Build Objects: Cortex-A53
#user@localhost:~$
cp -v ./CORTEXA/tispl.bin ./input/ ; \
cp -v ./CORTEXA/u-boot.img ./input/
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:
#user@localhost:~$
git clone https://github.com/RobertCNelson/ti-linux-kernel-dev ./kernelbuildscripts
cd kernelbuildscripts/
For ti-linux-arm64-6.6.y (Longterm 6.6.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/ti-linux-arm64-6.6.y -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
Root File System
Debian 13
| User | Password |
|---|---|
| debian | temppwd |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-13.1-base-arm64-2025-10-09.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-13.1-base-arm64-2025-10-09.tar.xz
#sha256sum output:
1cb10f5f49a488395caad40821fdfbdd3102a5b65d0a82d2ba34c3390652f8b8 debian-13.1-base-arm64-2025-10-09.tar.xz
Extract:
#user@localhost:~$
tar xf debian-13.1-base-arm64-2025-10-09.tar.xz
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Create Root File System with genimage:
The genimage https://github.com/pengutronix/genimage tool is now used to generate a sdcard.img vs directly interfacing with the microSD.
Host Package Requirements
#user@localhost:~$
sudo apt update ; \
sudo apt-get install -y dosfstools genimage mtools
Create working directory for genimage:
#user@localhost:~$
sudo mkdir -p ./input/.rootfs
Copy Root File System
#user@localhost:~$
sudo tar xfvp ./debian-*-*-arm64-*/arm64-rootfs-*.tar -C ./input/.rootfs/
sync
Enable first boot customization
#user@localhost:~$
sudo cp ./input/.rootfs/etc/bbb.io/templates/sysconf.txt ./input/
Open ./input/sysconf.txt in your text editor and change any user setting.
- user_name=
- user_password=
- hostname=
#user@localhost:~$
sudo nano ./input/sysconf.txt
Setup extlinux.conf
#user@localhost:~$
sudo sh -c "echo 'label Linux' > ./input/extlinux.conf"
sudo sh -c "echo ' kernel /Image.gz' >> ./input/extlinux.conf"
sudo sh -c "echo ' fdtdir /' >> ./input/extlinux.conf"
sudo sh -c "echo ' append console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=/dev/mmcblk1p2 ro rootfstype=ext4 fsck.repair=yes rootwait net.ifnames=0' >> ./input/extlinux.conf"
Copy Kernel Image
Kernel Image:
#user@localhost:~$
sudo cp -v ./kernelbuildscripts/deploy/${kernel_version}.Image ./input/Image.gz
Copy Kernel Device Tree Binaries
#user@localhost:~$
sudo mkdir -p ./input/dtbs/
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-dtbs.tar.gz -C ./input/dtbs/
sudo cp -v ./input/dtbs/ti/k3-am625-osd625-brk.dtb ./input/k3-am625-osd625-brk.dtb
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-modules.tar.gz -C ./input/.rootfs/usr/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk1p2 / auto errors=remount-ro 0 1' >> ./input/.rootfs/etc/fstab"
sudo sh -c "echo '/dev/mmcblk1p1 /boot/firmware vfat user,uid=1000,gid=1000,defaults 0 2' >> ./input/.rootfs/etc/fstab"
Check partition size
Verify Root File partition size, this can be used to modify the seek value below for size tweaking.
#user@localhost:~$
sudo du -sh ./input/.rootfs/
Create rootfs.ext4
#user@localhost:~$
sudo dd if=/dev/zero of=./input/rootfs.ext4 bs=1 count=0 seek=1600M
sudo mkfs.ext4 -F ./input/rootfs.ext4 -d ./input/.rootfs/
Create sdcard.img with genimage
The genimage https://github.com/pengutronix/genimage tool is now used to generate a sdcard.img vs directly interfacing with the microSD.
Create genimage.cfg file
#user@localhost:~$
nano genimage.cfg
#genimage.cfg
image boot.vfat {
vfat {
files = {
"tispl.bin",
"u-boot.img",
"Image.gz",
"sysconf.txt",
}
file tiboot3.bin {
image = "tiboot3-am62x-hs-fs-osd62x.bin"
}
file ti/k3-am625-osd625-brk.dtb {
image = "k3-am625-osd625-brk.dtb"
}
file extlinux/extlinux.conf {
image = "extlinux.conf"
}
}
size = 256M
}
image sdcard.img {
hdimage {}
partition u-boot {
partition-type = 0xC
bootable = "true"
image = "boot.vfat"
}
partition rootfs {
partition-type = 0x83
image = "rootfs.ext4"
}
}
Run genimage on genimage.cfg
#user@localhost:~$
sudo genimage --rootpath `mktemp` --config genimage.cfg
genimage output
sdcard.img can be flashed to a microSD using rpi-imager https://github.com/raspberrypi/rpi-imager or your favorite image writing software.
#user@localhost:~$
tree images/
images/
└── sdcard.img
1 directory, 1 file
Final Tweaks (extend rootfs partition)
Extend the rootfs partition to fill available space on drive.
Use growpart to extend a partition in a partition table
sudo growpart /dev/mmcblk1 2
voodoo@eewiki:~$ sudo growpart /dev/mmcblk1 2
CHANGED: partition=2 start=524289 old: size=3276800 end=3801088 new: size=61809630 end=62333918
First Reboot
sudo reboot
Use resize2fs to enlarge the existing filesystem
sudo resize2fs /dev/mmcblk1p2
voodoo@eewiki:~$ sudo resize2fs /dev/mmcblk1p2
resize2fs 1.47.0 (5-Feb-2023)
Filesystem at /dev/mmcblk1p2 is mounted on /; on-line resizing required
old_desc_blocks = 1, new_desc_blocks = 4
The filesystem on /dev/mmcblk1p2 is now 7726203 (4k) blocks long.
Second Reboot
This last reboot will take awhile as fsck is checking the partition on bootup.
sudo reboot
Comments
Any questions or comments please go to our TechForum: TechForum