Display Identification

Need to purchase multiple displays. They’re 1602 (16 characters 2 lines) however Im having difficulty and also want to make sure the ones Im purchasing have the 16 pins to connect to. Most seem to not come with that anymore. Any help would be appreciated. Thanks.

Welcome to the forum. It looks like part 3387-ACM1602K-NLW-BBW-ND is going to be the closest option to your original part. The version of the board is 3.8V instead of the 1.0V of your display. Here are options for the headers.