Do the LPR-02 Series Fuse Holders from Optifuse Include the Fuse

We often receive calls from customers wondering if the LPR-02 fuse holders from OptiFuse, such as the LPR-02B-18R, include the fuses. These fuse holders do not include the fuse. As indicated on the datasheet they are “For use with APR and ANR Regular (ATO/ATC Style) Blade Fuses”.

Please note that the current rating listed on the PDP is for the fuse holder itself, not for the fuse. Any compatible fuse up to the maximum amperage may be used.

Compatible fuses carried by DigiKey:
Fuses | Electronic Components Distributor DigiKey

Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
2298-LPR-02R-16R-ND LPR-02R-16R
2298-LPR-02B-16Y-ND LPR-02B-16Y
2298-LPR-02B-16B-ND LPR-02B-16B
2298-LPR-02B-14Y-ND LPR-02B-14Y
2298-LPR-02B-14B-ND LPR-02B-14B
2298-LPR-02B-14R-ND LPR-02B-14R
2298-LPR-02B-18R-LOOP-ND LPR-02B-18R-LOOP
2298-LPR-02B-12R-ND LPR-02B-12R
2298-LPR-02B-12B-ND LPR-02B-12B
2298-LPR-02B-16B-CU-ND LPR-02B-16B-CU
2298-LPR-02B-12OR-CU-ND LPR-02B-12OR-CU
2298-LPR-02B-14R-8-ND LPR-02B-14R-8
2298-LPR-02B-127Y-ND LPR-02B-127Y
2298-LPR-02B-18R-ND LPR-02B-18R
2298-LPR-02B-12OR-ND LPR-02B-12OR
2298-LPR-02B-12Y-ND LPR-02B-12Y
2298-LPR-02B-16R-ND LPR-02B-16R