Hi
Could we get some helping finding fuse for our trainer?
Have a nice day
Bob
Will fill in with some more information.
Hi
Could we get some helping finding fuse for our trainer?
Have a nice day
Bob
Will fill in with some more information.
Hi
Here is some more info.
Need fuses for 2 CIE Cleveland Institute of Electronics PLT-2 trainers.
Plus a CIE PLT-1 with Digital Training Lab add on.
Two have fuses for samples.
PLT–2’s call for a 300 mA fuses.
PLT-1 is unknown amperage .Cannot find a manual for it.
Two fuses are glass ones.
We can measure them in the morning.
Have a nice day
Bob
Can send pictures tomorrow too.
Welcome to the forum.
The glass fuses will most likely be one of the two most common sizes, 1-1/4" X 1/4" or 5X20mm.
The marking from the blown fuses and/or photos of them will help find the correct replacement.
Hi Paul
We will take care of the first PTL-2 we picked up first.
It was missing the fuse.
Give us a little bit to sort this out.
Have a nice day
Bob
Fuse from PTL-1 seems to fit it okay.
Will test fuse from second PTL-2 for fit.
Hi Paul
Here is the second PTL-2
It has a fuse in it.
Will measure it and give you part number on it.
Have a nice day
Bob
Hi Paul
The first measurement is 1 1/4 inch.
The 30 mm mark is a little past that so it seems like it is a 1 1/4 inch
Second measurement is 1/4 inch
6 mm is right around that
Reading part number is not working out
Would rather not.Causing pretty bad eye strain.
Silver label says 300 mA/250V/3AG
Also says ‘Regular Blow’
Hope that will do.
Have a nice day
Bob
Fuse holder is kind where cap holds fuse.
Use phillips to get it out.
Fuse stays with cap.Then you pull it out of cap.
Hello,
I only find fast blow or slo blow options. I am not aware of regular blow. List of options are below.
https://www.digikey.com/short/w3dtftvw
When in doubt use the fast blow. The fast blow is generally used for circuit board protection. Slow blow is more for motor start. If you try to use slow blow first, it could damage something if it is not fast enough. You can always change the fast blow if it is seems to be blowing the fuse all the time. The other way around can damage something.
You can actually look through the options for the fuse holders to see what you can make work. Here is the link: https://www.digikey.com/short/5qm9cb30
I could not narow it down any further. I provided the full link in case you need to check dimensions to make sure the option will fit where you need it to.
Hi Verna
Thank you.
A little misunderstanding here.
The fuse holder in this trainer is fine.
We have two PLT-2 trainers.
How we tell them apart is this has the fuse holder we described.
Will send pictures of fuseholder tomorrow morning.
Have a nice day
Bob
Regarding ‘Regular Blow’
This is late 60’s or 70’s trainer
Some ways of doing things may have fallen by the wayside.
Hi
So.Bottom line we just search Digikey for:
300 mA
3AG
We should never mind what the fuse holder looks like?
Have a nice day
Bob
Hi
We pick this one.
From Verna’s search.Thank you Verna.
https://www.digikey.com/en/products/detail/eaton-electronics-division/BK-AGC-3-10-R/954175
Is this a good one? It is fast blow.
Other fast blow was Littlefuse. Sounds like maybe better company but twice the price.
Have a nice day
Bob
Hello,
I am sorry. I am confused by the response . I gave short links above for bith items for you to review. You do have to right click on the link and click on open link. Though you should be able to see some choices to pick from.
Thank you Verna and David
Have a good evening
Bob