Does Omron have a waterproof model (IP67) with a small operating force (OF)?

Question:

Does Omron have a waterproof model (IP67) with a small operating force (OF)?

Block

Answer:

We have the following sealed basic switches with minimum OF, as shown in the catalog:
・D2VW: OF 1.96 N / 200 gf (pushbutton), 0.59 N / 60 gf (long hinge lever)
・D2SW: OF 1.77 N / 181 gf (pushbutton), 0.59 N / 60 gf (hinge lever)
・D2HW: OF 0.75 N / 77 gf (pushbutton), 0.50 N / 51 gf (long hinge lever)

Block

Explanation:

Due to the high airtightness of the sealed basic switch (IP67 specification), it is necessary to increase the release force (RF) compared to the open type because contraction of the internal air may delay the release when the temperature becomes low while it is being pushed in. As a result, sealed models generally require higher operating force than that of open types.

Block

Product category

Switches Basic Switches


Classification

Usage, Applications


Related keywords

Basic Switch
Sealed Basic Switch
IP67
Operating Force (OF)
Release Force (RF)

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ