Question:
Which basic switches are waterproof?
Answer:
Omron has basic switches with a degree of protection of IP67.
Explanation:
At IP67, water enters if the switch is opened and closed under water or the switch is continuously exposed to water. IP67 means that water does not enter if the product is submerged in water at a depth of 1 m for 30 minutes; it does not mean that the switch can be opened or closed under such an environment.
D2□W (W indicates support for IP67):
D2VW
D2SW
D2SW-P
D2FW-G
D2HW
D2JW
D2QW
D2AW
Product category
Switches Basic Switches
Classification
Selection, Characteristics
Related keywords
Basic Switch
Sealed Basic Switch
Dust
Dust-Proof
IP67
Waterproof
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
Which basic switches are waterproof? | FAQ | OMRON Device & Module Solutions - Americas