What is the sealing performance (waterproof, dustproof, gas resistance) of a basic switch?

Question:

What is the sealing performance (waterproof, dustproof, gas resistance) of a basic switch?

Block

Answer:

Omron basic switches have a lineup of IP40 to IP67 protective structures with waterproof and dustproof specifications conforming to the protective structure. We have sealed basic switches with IP67. Please note that we do not have standards for gas resistance.

Explanation:

For some models we can provide test data for reference only. Accelerated test data cannot evaluate how many equivalent years correspond in the actual environment.
Do not use the product in an atmosphere with high temperature and humidity or in a harmful gas such as sulfide gas (H2S, SO2), ammonia gas (NH3), nitric acid gas (HNO3) or chlorine gas (Cl2). It may cause malfunction such as contact failure or damage due to corrosion.


Product category Switches Basic Switches

Switches Basic Switches
Switches Basic Switches


Classification Usage,Applications
Usage, Applications


Related keywords

Basic Switch
Sealed Basic Swich
Protective Structure
IP40 IP67
Water Resistance
Dust Resistance
Gas Resistance

Block

Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/switches/FAQE20030