Question:
What are corrosion-resistant basic switches?
![]()
Answer:
There are various types of corrosion and Omron’s basic switches have various specifications such as gold contacts, sealed structures, and built-in reed switches that will help prevent corrosion. Select proper specification as needed.
![]()
Explanation:
Oxidation and sulfurization of silver contacts are inevitable due to the external environment. However, it is possible to reduce the influence by using gold contacts, sealed structures, and built-in reed switches.
The criteria for the environment cannot be defined. It is recommended to perform evaluation under actual usage with the following types of switches:
Those that use gold contacts (0.1A rating or microload switching compatible product)
Sealed basic switch (less susceptible to external environmental influences because its structure prevents water from entering)
Built-in reed switch type (D2RV)
Note that the metal parts other than contacts are affected.
![]()
Product category
Switches Basic Switches
Classification
Selection, Characteristics
Related keywords
Basic Switch
Gold Contact
Silver Contact
IP67
Oxidation
Sulfidation
Buit-in Reed Switch
![]()
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/switches/FAQE20012