Efficient MOSFET Drive Techniques: Push-Pull and Bootstrap Topologies for High-Speed Switching

In our previous article, we discussed basic drive topologies such as low-side and high-side MOSFET drive configurations. However, as power devices evolve toward higher switching speeds and improved efficiency, traditional low- and high-side drive topologies may fall short in terms of performance and reliability.

In such scenarios, advanced drive topologies like push-pull and bootstrap drive offer optimized solutions, along with several additional application benefits.

This article focuses on two important drive configurations: push-pull drive and bootstrap drive, exploring their working principles, advantages, design considerations, and practical use cases.

1. Push-Pull Drive

A push-pull drive consists of two MOSFETs or bipolar transistors forming a complementary output pair, alternately driving the gate voltage up or down.

It is suitable for gate driver IC output stages (e.g., Microchip TC4420 and TC4429), high-frequency/high-current switching drives (e.g., PWM control, motor control), and similar applications.

Advantages

  • Fast switching Speed (fast charging/discharging of gate capacitance)
  • Strong drive capability (>2A)
  • Reduced crossover losses

Limitations

  • Requires careful dead-time management to prevent shoot-through current
  • Slightly more expensive, complex to control

Design Considerations

  • 1. Shoot-through Prevention
    In the design considerations for push-pull drivers, it is important to prevent shoot-through.
    In a push-pull configuration, the two drivers need to alternate conduction; if an appropriate dead time is not set, it may result in both the upper and lower drivers conducting simultaneously, causing a short circuit.

  • 2. Controlled Switching Speed
    Excessive switching speed can lead to electromagnetic interference (EMI) and oscillation. By adjusting the gate resistor value, the switching speed can be controlled, thereby reducing EMI.

  • 3. Appropriate drive current
    Select an appropriate drive current based on the MOSFET’s gate charge and required switching speed. Ensure the driver has sufficient current capability to charge/discharge the gate quickly.

  • 4. PCB layout
    For PCB layout, minimize parasitic inductance and capacitance in the drive path to maintain signal integrity and avoid EMI issues.

Tech Tip: Half-bridge drivers usually include circuitry to prevent shoot-through. However, additional dead-time delays may be required. This can be achieved by including limits on the associated microcontroller’s PWM signal.

On a related note, be sure to limit the PWM duty cycle to allow time for the bootstrap capacitor to charge.

Example Circuit: Transistor-Based Push-Pull Drive


Example of transistor low-side push-pull drive circuit

In the example above, a transistor-based low-side push-pull drive circuit is shown. Transistors such as 8050 or 8550, or B772 and D882, can be used. The test power supply here is DC 12V, so no additional drive voltage is needed. If the load voltage exceeds the control voltage, the drive voltage must be reduced to stay within the MOSFET’s Vgs limits.

Recommended ICs:

2. Bootstrap drive

A bootstrap drive uses a capacitor to store the voltage difference when the low-side MOSFET is on, then uses this voltage to drive the high-side N-MOSFET.
It is suitable for half-bridge or full-bridge circuits (e.g., inverters, motor drives) and scenarios requiring elevated Vgs for high-side MOSFETs.

Advantages

  • Lower Rds(on) for higher efficiency (uses N-MOSFETs for high-side switching )
  • Compact and cost-effective

Limitations

  • Cannot maintain continuous high-side ON time
  • Needs periodic low-side conduction to recharge bootstrap capacitor
  • Limited by PWM duty cycle (sufficient time must be allocated for capacitor charging)

Design Considerations

  • 1. Bootstrap Capacitor Selection (C_boot)
    Its capacitance should be at least 10 times the high-side MOSFET’s gate capacitance to ensure sufficient charge during switching. Use multilayer ceramic capacitors (MLCC) with low equivalent series resistance (ESR) and inductance (ESL) to reduce voltage ripple and improve reliability.

  • 2. Bootstrap Diode Selection
    Choose a Schottky diode with low forward voltage drop and fast recovery to minimize power loss and improve switching speed.

  • 3. Bootstrap Resistor (R_boot)
    Include a bootstrap resistor (R_boot) to limit peak current during startup, protecting the diode. Balance the resistor value between charging time and current limiting to avoid excessive delay or high inrush current.

  • 4. PCB layout
    Place the bootstrap capacitor and diode as close as possible to the driver IC to minimize parasitic inductance and resistance. Reduce loop area for high-current paths to lower EMI and voltage spikes.

  • 5. Conduction Time Limitation
    Bootstrap circuits are unsuitable for prolonged high-side MOSFET conduction, as the capacitor may not sustain sufficient voltage. For low-frequency or static applications, consider isolated drive solutions.

Example Circuit: Bootstrap-Based High-Side Drive


Example of MOSFET bootstrap drive circuit

The example above shows a simplified high-side MOSFET gate drive circuit for brushed or brushless motor H-bridges or three-phase H-bridges.
Bootstrap capacitor C1 supplies energy for gate drive, sourced directly from the optocoupler’s output transistor. The circuit uses a common-collector configuration, with an NPN transistor pulling the MOSFET gate up to the bootstrap voltage. During turn-off, resistor R2 discharges the MOSFET gate through current-limiting resistor R4.

Recommended ICs

TI UCC27710

Infineon EiceDRIVER Series

Drive Topology Comparison Table

Drive Topology Applicable Scenarios Advantages Disadvantages Common IC Solutions
Push-Pull High-frequency switching, digital circuits High drive current, fast switching Requires precise dead-time control Microchip TC4420、TC4429
Bootstrap Half/full-bridge, high-side switching No isolation power needed, low cost High-side conduction time limited, bootstrap cap sizing critical TI UCC27710、Infineon EiceDRIVER

Conclusion

Push-pull and bootstrap drive topologies offer solutions for fast, efficient MOSFET switching. Push-pull drives are great for high-speed control with strong gate drive, while bootstrap circuits let you use N-MOSFETs on the high side without needing a separate power supply.

Each has its strengths - and limitations - so understanding when and how to use them is key to building reliable power circuits. In our next article, we’ll explore opto-isolated and bridge drives, perfect for high-voltage and complex motor control setups.

Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
TC4420COA713TR-ND,TC4420COA713CT-ND,TC4420COA713DKR-ND TC4420COA713
TC4420EOA-ND TC4420EOA
TC4420COA-ND TC4420COA
TC4420EPA-ND TC4420EPA
TC4420VPA-ND TC4420VPA
TC4420CPA-ND TC4420CPA
TC4420CAT-ND TC4420CAT
TC4420VOA713TR-ND,TC4420VOA713CT-ND,TC4420VOA713DKR-ND TC4420VOA713
TC4420VOA-ND TC4420VOA
TC4420EOA713TR-ND,TC4420EOA713CT-ND,TC4420EOA713DKR-ND TC4420EOA713
TC4420MJA-ND TC4420MJA
TC4420IJA-ND TC4420IJA
TC4420EMF713-ND TC4420EMF713
TC4420EMF-ND TC4420EMF
TC4420VMF-ND TC4420VMF
TC4420VMF713-ND TC4420VMF713
TC4420VAT-ND TC4420VAT
TC4429EOA-ND TC4429EOA
TC4429CPA-ND TC4429CPA
TC4429COA713TR-ND,TC4429COA713CT-ND,TC4429COA713DKR-ND TC4429COA713
TC4429VOA-ND TC4429VOA
TC4429COA-ND TC4429COA
TC4429EPA-ND TC4429EPA
TC4429CAT-ND TC4429CAT
TC4429VMF-ND TC4429VMF
TC4429VPA-ND TC4429VPA
TC4429EMF-ND TC4429EMF
TC4429EMF713-ND TC4429EMF713
TC4429VMF713-ND TC4429VMF713
TC4429EOA713-ND TC4429EOA713
TC4429VOA713-ND TC4429VOA713
TC4429VAT-ND TC4429VAT
TC4429MJA-ND TC4429MJA
TC4429IJA-ND TC4429IJA
296-52844-2-ND,296-52844-1-ND,296-52844-6-ND UCC27710DR
296-47513-ND UCC27710D
1EDN8511BXUSA1TR-ND,1EDN8511BXUSA1CT-ND,1EDN8511BXUSA1DKR-ND 1EDN8511BXUSA1
2EDN7524FXTMA1TR-ND,2EDN7524FXTMA1CT-ND,2EDN7524FXTMA1DKR-ND 2EDN7524FXTMA1
2EDN7524GXTMA1TR-ND,2EDN7524GXTMA1CT-ND,2EDN7524GXTMA1DKR-ND 2EDN7524GXTMA1
2EDL05N06PFXUMA1TR-ND,2EDL05N06PFXUMA1CT-ND,2EDL05N06PFXUMA1DKR-ND 2EDL05N06PFXUMA1
448-2EDL8024GXUMA1TR-ND,448-2EDL8024GXUMA1CT-ND,448-2EDL8024GXUMA1DKR-ND 2EDL8024GXUMA1
448-2EDF7275FXUMA2TR-ND,448-2EDF7275FXUMA2CT-ND,448-2EDF7275FXUMA2DKR-ND 2EDF7275FXUMA2
448-2ED2410EMXUMA1TR-ND,448-2ED2410EMXUMA1CT-ND,448-2ED2410EMXUMA1DKR-ND 2ED2410EMXUMA1
2ED020I12F2XUMA1TR-ND,2ED020I12F2XUMA1CT-ND,2ED020I12F2XUMA1DKR-ND 2ED020I12F2XUMA1
448-2EDN7534FXTMA1TR-ND,448-2EDN7534FXTMA1CT-ND,448-2EDN7534FXTMA1DKR-ND 2EDN7534FXTMA1
448-2EDN8534FXTMA1TR-ND,448-2EDN8534FXTMA1CT-ND,448-2EDN8534FXTMA1DKR-ND 2EDN8534FXTMA1
1EDN7511BXUSA1TR-ND,1EDN7511BXUSA1CT-ND,1EDN7511BXUSA1DKR-ND 1EDN7511BXUSA1
1EDN7550BXTSA1TR-ND,1EDN7550BXTSA1CT-ND,1EDN7550BXTSA1DKR-ND 1EDN7550BXTSA1
1EDN8550BXTSA1TR-ND,1EDN8550BXTSA1CT-ND,1EDN8550BXTSA1DKR-ND 1EDN8550BXTSA1
1EDN7512GXTMA1TR-ND,1EDN7512GXTMA1CT-ND,1EDN7512GXTMA1DKR-ND 1EDN7512GXTMA1
448-1EDN9550BXTSA1TR-ND,448-1EDN9550BXTSA1CT-ND,448-1EDN9550BXTSA1DKR-ND 1EDN9550BXTSA1
2EDN8524FXTMA1TR-ND,2EDN8524FXTMA1CT-ND,2EDN8524FXTMA1DKR-ND 2EDN8524FXTMA1
448-2EDN7524RXTMA1TR-ND,448-2EDN7524RXTMA1CT-ND,448-2EDN7524RXTMA1DKR-ND 2EDN7524RXTMA1
448-2EDN7534BXTSA1TR-ND,448-2EDN7534BXTSA1CT-ND,448-2EDN7534BXTSA1DKR-ND 2EDN7534BXTSA1
448-1EDL8011XUMA1TR-ND,448-1EDL8011XUMA1CT-ND,448-1EDL8011XUMA1DKR-ND 1EDL8011XUMA1
2EDL05I06PJXUMA1TR-ND,2EDL05I06PJXUMA1CT-ND,2EDL05I06PJXUMA1DKR-ND 2EDL05I06PJXUMA1
2EDL23N06PJXUMA1TR-ND,2EDL23N06PJXUMA1CT-ND,2EDL23N06PJXUMA1DKR-ND 2EDL23N06PJXUMA1
448-2EDS7165HXUMA1TR-ND,448-2EDS7165HXUMA1CT-ND,448-2EDS7165HXUMA1DKR-ND 2EDS7165HXUMA1
448-2EDF8275FXUMA1TR-ND,448-2EDF8275FXUMA1CT-ND,448-2EDF8275FXUMA1DKR-ND 2EDF8275FXUMA1
2EDF7275KXUMA1TR-ND,2EDF7275KXUMA1CT-ND,2EDF7275KXUMA1DKR-ND 2EDF7275KXUMA1
448-2EDF7275KXUMA2TR-ND,448-2EDF7275KXUMA2CT-ND,448-2EDF7275KXUMA2DKR-ND 2EDF7275KXUMA2
448-2EDF9275FXUMA1TR-ND,448-2EDF9275FXUMA1CT-ND,448-2EDF9275FXUMA1DKR-ND 2EDF9275FXUMA1
6EDL04N02PRXUMA1TR-ND,6EDL04N02PRXUMA1CT-ND,6EDL04N02PRXUMA1DKR-ND 6EDL04N02PRXUMA1
448-2EDS8265HXUMA2TR-ND,448-2EDS8265HXUMA2CT-ND,448-2EDS8265HXUMA2DKR-ND 2EDS8265HXUMA2
448-1EDN7550UXTSA1TR-ND,448-1EDN7550UXTSA1CT-ND,448-1EDN7550UXTSA1DKR-ND 1EDN7550UXTSA1
448-2EDN7434FXTMA1TR-ND,448-2EDN7434FXTMA1CT-ND,448-2EDN7434FXTMA1DKR-ND 2EDN7434FXTMA1
448-2EDN8533FXTMA1TR-ND,448-2EDN8533FXTMA1CT-ND,448-2EDN8533FXTMA1DKR-ND 2EDN8533FXTMA1
448-2EDN7533RXTMA1TR-ND,448-2EDN7533RXTMA1CT-ND,448-2EDN7533RXTMA1DKR-ND 2EDN7533RXTMA1
448-2EDN8534RXTMA1TR-ND,448-2EDN8534RXTMA1CT-ND,448-2EDN8534RXTMA1DKR-ND 2EDN8534RXTMA1
448-2EDN7534RXTMA1TR-ND,448-2EDN7534RXTMA1CT-ND,448-2EDN7534RXTMA1DKR-ND 2EDN7534RXTMA1
2EDN7424FXTMA1TR-ND,2EDN7424FXTMA1CT-ND,2EDN7424FXTMA1DKR-ND 2EDN7424FXTMA1
2EDN7523FXTMA1TR-ND,2EDN7523FXTMA1CT-ND,2EDN7523FXTMA1DKR-ND 2EDN7523FXTMA1
448-2EDN7533BXTSA1TR-ND,448-2EDN7533BXTSA1CT-ND,448-2EDN7533BXTSA1DKR-ND 2EDN7533BXTSA1
448-2EDN8524RXTMA1TR-ND,448-2EDN8524RXTMA1CT-ND,448-2EDN8524RXTMA1DKR-ND 2EDN8524RXTMA1
448-2EDL8123GXUMA1TR-ND,448-2EDL8123GXUMA1CT-ND,448-2EDL8123GXUMA1DKR-ND 2EDL8123GXUMA1
448-2EDL8124GXUMA1TR-ND,448-2EDL8124GXUMA1CT-ND,448-2EDL8124GXUMA1DKR-ND 2EDL8124GXUMA1
2EDL05I06PFXUMA1TR-ND,2EDL05I06PFXUMA1CT-ND,2EDL05I06PFXUMA1DKR-ND 2EDL05I06PFXUMA1
2EDL05I06BFXUMA1TR-ND,2EDL05I06BFXUMA1CT-ND,2EDL05I06BFXUMA1DKR-ND 2EDL05I06BFXUMA1
448-2EDL8033G4CXTMA1TR-ND,448-2EDL8033G4CXTMA1CT-ND,448-2EDL8033G4CXTMA1DKR-ND 2EDL8033G4CXTMA1
448-2EDL8034G3CXTMA1TR-ND,448-2EDL8034G3CXTMA1CT-ND,448-2EDL8034G3CXTMA1DKR-ND 2EDL8034G3CXTMA1
448-2EDL8033G3CXTMA1TR-ND,448-2EDL8033G3CXTMA1CT-ND,448-2EDL8033G3CXTMA1DKR-ND 2EDL8033G3CXTMA1
448-2EDL8023GXUMA1TR-ND,448-2EDL8023GXUMA1CT-ND,448-2EDL8023GXUMA1DKR-ND 2EDL8023GXUMA1
2EDL05N06PJXUMA1TR-ND,2EDL05N06PJXUMA1CT-ND,2EDL05N06PJXUMA1DKR-ND 2EDL05N06PJXUMA1
448-2EDS8165HXUMA2TR-ND,448-2EDS8165HXUMA2CT-ND,448-2EDS8165HXUMA2DKR-ND 2EDS8165HXUMA2
448-2EDS9265HXUMA1TR-ND,448-2EDS9265HXUMA1CT-ND,448-2EDS9265HXUMA1DKR-ND 2EDS9265HXUMA1
448-2EDF7175FXUMA2TR-ND,448-2EDF7175FXUMA2CT-ND,448-2EDF7175FXUMA2DKR-ND 2EDF7175FXUMA2
6EDL04N06PTXUMA1TR-ND,6EDL04N06PTXUMA1CT-ND,6EDL04N06PTXUMA1DKR-ND 6EDL04N06PTXUMA1
6EDL04I06PTXUMA1TR-ND,6EDL04I06PTXUMA1CT-ND,6EDL04I06PTXUMA1DKR-ND 6EDL04I06PTXUMA1
6EDL04I06NTXUMA1TR-ND,6EDL04I06NTXUMA1CT-ND,6EDL04I06NTXUMA1DKR-ND 6EDL04I06NTXUMA1
6ED003L06F2XUMA1TR-ND,6ED003L06F2XUMA1CT-ND,6ED003L06F2XUMA1DKR-ND 6ED003L06F2XUMA1
2ED020I12FAXUMA2TR-ND,2ED020I12FAXUMA2CT-ND,2ED020I12FAXUMA2DKR-ND 2ED020I12FAXUMA2
448-1EDN7136GXTMA1TR-ND,448-1EDN7136GXTMA1CT-ND,448-1EDN7136GXTMA1DKR-ND 1EDN7136GXTMA1
448-2EDN8533RXTMA1TR-ND,448-2EDN8533RXTMA1CT-ND,448-2EDN8533RXTMA1DKR-ND 2EDN8533RXTMA1
448-2EDN7434RXTMA1TR-ND,448-2EDN7434RXTMA1CT-ND,448-2EDN7434RXTMA1DKR-ND 2EDN7434RXTMA1
448-1EDN7146GXTMA1TR-ND,448-1EDN7146GXTMA1CT-ND,448-1EDN7146GXTMA1DKR-ND 1EDN7146GXTMA1
448-2EDN7424RXTMA1TR-ND,448-2EDN7424RXTMA1CT-ND,448-2EDN7424RXTMA1DKR-ND 2EDN7424RXTMA1
448-2EDN8524GXTMA1TR-ND,448-2EDN8524GXTMA1CT-ND,448-2EDN8524GXTMA1DKR-ND 2EDN8524GXTMA1
448-2EDL8034G4CXTMA1TR-ND,448-2EDL8034G4CXTMA1CT-ND,448-2EDL8034G4CXTMA1DKR-ND 2EDL8034G4CXTMA1
448-2EDL8034G4BXTMA1TR-ND,448-2EDL8034G4BXTMA1CT-ND,448-2EDL8034G4BXTMA1DKR-ND 2EDL8034G4BXTMA1
2EDL23I06PJXUMA1TR-ND,2EDL23I06PJXUMA1CT-ND,2EDL23I06PJXUMA1DKR-ND 2EDL23I06PJXUMA1
6ED003L02F2XUMA1TR-ND,6ED003L02F2XUMA1CT-ND,6ED003L02F2XUMA1DKR-ND 6ED003L02F2XUMA1
1EBN1001AEXUMA1TR-ND,1EBN1001AEXUMA1CT-ND,1EBN1001AEXUMA1DKR-ND 1EBN1001AEXUMA1
448-2EDL8033F5BXUMA1TR-ND,448-2EDL8033F5BXUMA1CT-ND,448-2EDL8033F5BXUMA1DKR-ND 2EDL8033F5BXUMA1
448-2EDL8034F5BXUMA1TR-ND,448-2EDL8034F5BXUMA1CT-ND,448-2EDL8034F5BXUMA1DKR-ND 2EDL8034F5BXUMA1
448-2EDL5023U2DXTMA1TR-ND,448-2EDL5023U2DXTMA1CT-ND,448-2EDL5023U2DXTMA1DKR-ND 2EDL5023U2DXTMA1
448-2EDL5013U2DXTMA1TR-ND,448-2EDL5013U2DXTMA1CT-ND,448-2EDL5013U2DXTMA1DKR-ND 2EDL5013U2DXTMA1
2EDN8524RXUMA1TR-ND,2156-2EDN8524RXUMA1-ND 2EDN8524RXUMA1
448-1EDN7126GXTMA1TR-ND,448-1EDN7126GXTMA1CT-ND,448-1EDN7126GXTMA1DKR-ND 1EDN7126GXTMA1
2EDN8523FXTMA1TR-ND,2EDN8523FXTMA1CT-ND,2EDN8523FXTMA1DKR-ND,2156-2EDN8523FXTMA1-ND 2EDN8523FXTMA1
2EDN7523RXUMA1TR-ND,2EDN7523RXUMA1CT-ND,2EDN7523RXUMA1DKR-ND,2156-2EDN7523RXUMA1-ND 2EDN7523RXUMA1
2EDN8523RXUMA1TR-ND,2EDN8523RXUMA1CT-ND,2EDN8523RXUMA1DKR-ND,2156-2EDN8523RXUMA1-ND 2EDN8523RXUMA1
448-2EDL8114GXUMA1TR-ND,2156-2EDL8114GXUMA1-ND 2EDL8114GXUMA1
448-2EDS8265HXUMA3TR-ND,448-2EDS8265HXUMA3CT-ND,448-2EDS8265HXUMA3DKR-ND 2EDS8265HXUMA3
2EDF7235KXUMA1TR-ND,2EDF7235KXUMA1CT-ND 2EDF7235KXUMA1
448-1EDN6550BXTSA1TR-ND,448-1EDN6550BXTSA1CT-ND,448-1EDN6550BXTSA1DKR-ND 1EDN6550BXTSA1
448-2EDN7533FXTMA1TR-ND,448-2EDN7533FXTMA1CT-ND,448-2EDN7533FXTMA1DKR-ND 2EDN7533FXTMA1
448-2EDF7175FXUMA1TR-ND,2156-2EDF7175FXUMA1-ND 2EDF7175FXUMA1
1EDN7512BXTSA1TR-ND,1EDN7512BXTSA1CT-ND,1EDN7512BXTSA1DKR-ND 1EDN7512BXTSA1
448-1EDN7116GXTMA1TR-ND,448-1EDN7116GXTMA1CT-ND,448-1EDN7116GXTMA1DKR-ND 1EDN7116GXTMA1
448-1EDB9275FXUMA1TR-ND,448-1EDB9275FXUMA1CT-ND,448-1EDB9275FXUMA1DKR-ND 1EDB9275FXUMA1
448-2EDN7534UXTSA1TR-ND 2EDN7534UXTSA1
448-2EDN7534GXTMA1TR-ND,448-2EDN7534GXTMA1CT-ND,448-2EDN7534GXTMA1DKR-ND 2EDN7534GXTMA1
448-2EDN8523RXTMA1TR-ND,448-2EDN8523RXTMA1CT-ND,448-2EDN8523RXTMA1DKR-ND 2EDN8523RXTMA1
448-1EBN1002AEXUMA1TR-ND 1EBN1002AEXUMA1
2EDS8165HXUMA1TR-ND,2EDS8165HXUMA1CT-ND,2EDS8165HXUMA1DKR-ND 2EDS8165HXUMA1
2EDF7275FXUMA1TR-ND,2EDF7275FXUMA1CT-ND,2EDF7275FXUMA1DKR-ND 2EDF7275FXUMA1
448-6EDL04I06NCX1SA1-ND 6EDL04I06NCX1SA1
448-6EDL04I06PCX1SA1-ND 6EDL04I06PCX1SA1
448-6EDL04N06PCX1SA1-ND 6EDL04N06PCX1SA1
2EDS8265HXUMA1TR-ND,2EDS8265HXUMA1CT-ND,2EDS8265HXUMA1DKR-ND 2EDS8265HXUMA1
2EDN7524RXUMA1TR-ND 2EDN7524RXUMA1
448-2EDN7523GXTMA1TR-ND,448-2EDN7523GXTMA1CT-ND,448-2EDN7523GXTMA1DKR-ND 2EDN7523GXTMA1
2EDN7424RXUMA1TR-ND 2EDN7424RXUMA1
1EDN7511BXTSA1-ND 1EDN7511BXTSA1
1EDN8511BXTSA1-ND 1EDN8511BXTSA1
448-2EDN8523GXTMA1TR-ND,448-2EDN8523GXTMA1CT-ND,448-2EDN8523GXTMA1DKR-ND 2EDN8523GXTMA1
2EDS8155HXUMA1-ND 2EDS8155HXUMA1
2EDS8255HXUMA1-ND 2EDS8255HXUMA1
448-2EDL8112GXUMA1TR-ND 2EDL8112GXUMA1
448-2EDL8013GXUMA1TR-ND 2EDL8013GXUMA1
448-2EDN7523RXTMA1TR-ND,448-2EDN7523RXTMA1CT-ND,448-2EDN7523RXTMA1DKR-ND 2EDN7523RXTMA1
448-2EDN7433BXTSA1TR-ND,448-2EDN7433BXTSA1CT-ND,448-2EDN7433BXTSA1DKR-ND 2EDN7433BXTSA1
448-2EDL8014GXUMA1TR-ND 2EDL8014GXUMA1
448-2EDN7434BXTSA1TR-ND,448-2EDN7434BXTSA1CT-ND,448-2EDN7434BXTSA1DKR-ND 2EDN7434BXTSA1
448-2EDL8012GXUMA1TR-ND 2EDL8012GXUMA1
448-2EDL8113GXUMA1TR-ND 2EDL8113GXUMA1