Hi!
The Blackfly S cameras, e.g. BFS-PGE-63S4M-C, https://www.digikey.se/en/products/detail/flir-integrated-imaging-solutions-inc/BFS-PGE-63S4M-C/16528290, are illustrated with a camera visibly a USB 3.1 interface, but in the specifications and as well in the data sheet, Box, the label is GigE PoE. Are both interfaces available for purchase, or just one, and in that case which is the current being sold?
The USB options are 4331-BFS-U3-63S4M-C-ND and 4331-BFS-U3-63S4C-C-ND. By changing the PGE to U3 it changes the connection type for the camera.
Here are all of the Blackfly S options that are available.