We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I want to build an LED grow lighting using this particular strip. I want to link 8 of these strip together with heat sink but I want to know what Driver is compatible(wattage,volt) with this set up.
The nominal rated input power for each strip is approximately 100 watts; were one to drive 8 of them in parallel from a HLG-320H-48B for example, the configuration should be valid and workable, but each strip would operate at approximately 840mA of drive current, or just slightly over 1/3rd of their intended drive level.
Such a configuration may be advantageous in terms of creating a physically expansive array and/or reducing thermal management concerns, but at day’s end in doing so one would be buying about $200 worth of LEDs more than would be needed otherwise for a more or less equivalent light output.
If you want to run 8 of those strips at nominal input power, a pair of HLG-480H-54 should be suitable. (Very) loosely speaking, that should offer an approximation of direct sunlight over an area approximately 2’x4’ in size.
So I wanna build something like this. There is 8 bars, each bar is roughly 46inches. I am assuming each bar can attach 2 LED strips. That means this build will required 16 led strips? What driver will i need to build something like this pic i have above. Thanks for the input you guys.
Choose how much light you want; use enough LEDs to get there, and enough drivers to power them.
In context of prior discussion,that would translate into a 1.6kW array; roughly the equivalent of common electric space heaters. Thermal management seems likely to become problematic. Consider starting with half that, leaving provisions for expansion if needed.
I understand what you’re saying. I’m just trying to replicate these grow LED thats in the market. Are they using a special driver to operate such fixtures because the amount of driver needed to run a 5x5 coverage LED fixture is a lot
Another option may be 1145-USCO-320210GA-ND to power 4 strips wired in series connection.
It could be they use a custom driver specially manufactured for their design. Although initially expensive to create, custom designs save money on a mass production scale.