Product: IWR1642
Operating System: Raspberry pi
Steps executed from the below link
I am using the below-mentioned steps to execute the Out Of Box Demo with the IWR1642 radar. I have modified the code for storing the detection of objects and plotting the results in the output. On executing the code with the raspberry pi. I have made some observations. Requesting someone to kindly resolve the issue.
- How to pass the advance frame config into the python code. As mentioned in the below code under mmwave_nav.py in the run_demo method
if reconfig:
print("Sending configuration command...")
interface.send_item(interface.control_tx_queue, 'advFrameCfg\n')
- I have also observed that none is getting printed in the output of the receive data from the radar
def recv_item(rx_q):
# Fetch one line or frame from the rx buffer
return rx_q.get() if not rx_q.empty() else None