Going to buy FSP-FC210 but some question arised

Regarding to

I had asked some question via live chat support, and have a question left.

In datasheet, the maximum the PDB support is 2400w, but on the product page’s description it’s labeled 2524w. So, what actual the power capacity of this unit is ?

Since it has 2 Power Supply Unit, do they have 2524w each (for redundancy), or is it a total of 2 Units combined ?

Hello,

Welcome to the TechForum!

After looking over the datasheet I see this part as having a combined power of 2372W or RMS. This is capable of higher loads for short times and in a test setting this one could make up to 2524W max for a brief period but don’t count on a long lifespan.

I see this part states 500,000 hours of continuous operation at 55°C, 100% output load so this will run at that 2372W for longest life.

Hopefully this helps and feel free to follow up anytime.

Thank you

Ryan