GRACO SPRAYER X21

I have a GRACO SPRAYER X21 on which the SMD resistors R1 and R9 on the printed circuit board are burnt out so that their value cannot be identified. The supply voltage is 220VAC. Can someone send me a photo of the correct printed circuit board? The SMD resistors are located under the small PCB board with the fuse.

I am not able to visibly see any markings on the picture provided in order to identify the value of the resistors. You will need to contact Graco to see if they can provide the original schematic for this sprayer PCB