Hand Crimp tool for DF53-32PCF?

------Question for DF53-32PCF Please Put your question below------

Is there a Hand Crimp tool for DF53-32PCF?

Unfortunately the only crimp tool recommended by Hirose is part number CM-105C-ND, which is a bench mounted press. This is fairly typical for contacts that are manufactured on a reel.

Thanks for the reply! I did see that machine, but was curious since I the part can be sold in cut tape in lower quantities that maybe there was a hand tool for it.

Particularly with terminals this small, manufacturer-endorsed hand crimp tools are often unavailable due to the increasing effect of user factors in achieving a successful crimp, and the rapid rate at which machine tooling pays for itself in reduced labor and waste.

That said, these do appear to be of a common “F-crimp” format for which “universal” tools do exist to address one-off/hobby/repair scenarios.

Use of such tools is of course at the user’s risk and not recommended for production. The crimp-related documents on the manufacturer’s product page may be found helpful in evaluating the result if one chooses to do so.

Thank you very much for taking the time to reply and to explain. It is much appreciated!