I am working on fixing a fairly expensive piece of equipment that has a damaged motor controller. I have a controller that will work with it (already tested it), but I don’t want to just cut the connectors off and solder the wires to the board.
From the best I can gather digging around on the internet all these are some kind of JST connector. The first 2 pictures are just a three pin connector, male and female. I assume the third one is just a 2 pin version of the three pin connector. The fourth is bit smaller and a slightly different style. I’ll probably buy these from Digikey so links to the parts would be great.
Well I did have the third picture here, till they told me I can only post three pictures … so you’ll have to use a sixth sense or some other hocus-pocus. This is why I HATE finding parts on the internet. Been working on this for a week and I haven’t even placed an order yet. And after waiting 7 days for said order, I’ll find out I ordered the wrong thing, take a week or 2 to find the right thing, order more parts. And somewhere around a month after starting this I will have it fixed something that would have taken ONE day previously.