Help me find this Part?

This part of my laptop Mosfet 3 weeks ago blowed up and now I cant find which one to buy because the mosfet is destroyed and the labels are destroyed too. I found it on the Motherboard near the CPU. I think it is a N channel mosfet.



My laptop is Asus Tuf FA507RE, I couldn’t get the schematics of the laptop. Please help me.

Are these two transistors the same?
If so, it is PJX8838.
X38 - Panjit-PJX8838.pdf (399,4 КБ)

The only reason I am going to say it might not be is The Blown Mosfet has a lot bent legs and I think it is a SOT-23-6 Mosfet while The PJX8838 is not bent that much and it is a SOT-563.

What letters can be read on the marking?
Take a large photo from different sides of the burnt transistor.

The only thing I can see is N and either a U or a V. 6 pins and both side pins come from the body which makes me think it is a sot-23-6

What is the marking code on these elements (parts)?

The first one the remark is unreadable. second one it is either x34 or 36. Third one I can only see bars forth and fifth are like the second either x34 or 36.

Hello,
Welcome to the DigiKey TechForum. I’m not able to find any information on these part markings.

Thanks for trying man. Really Appreciate it

I have found some remarks of the Blown Transistor. You can see the photo and also it has N:N 144 so If that helps

zubiyrbozri

Sorry I am not finding anything with the markings in the picture for a transistor .

Thanks Craig

Take a picture of the entire motherboard from both sides. I need to see some details.

I almost found the answer, but I need photos of the board from both sides.

Bingo!
Finally I found it.
It’s SSM6N7002KFU.

Very nice find, there @Adam7!

sorry man. There was no Electricity so I wasn’t active Thanks for the Help.

You are Welcome!