Question:
How long can a relay withstand a momentary power interruption?
![]()
Answer:
There is no specified time for momentary power interruption. It depends on the circuit and equipment you use.
Please check with the actual equipment.
![]()
Explanation:
Release time is listed, but this is not the same amount of time to withstand an instantaneous blackout.
For example, if the “release time is less than or equal to 25 ms,” the voltage is cut off and the motor is always restored within 25 ms.
Both AC and DC coils may be released even if the momentary power interruption lasts for a shorter time than the specified maximum value of release time.
![]()
Quick tips
If the transition of contact state due to momentary power interruption is a problem, contact operation can be prevented by using a latching relay.
![]()
Please visit the link below to see this product line on the Digi-Key website
Relays | Digi-Key Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10043