For this post we will assume you have already loaded the latest version of the Arduino PLC IDE. We will also assume you have connected the Arduino Opta to your PC via the type C USB connector.
-
Start by verifying the Arduino Opta is recognized by your PC. This can be done via the Windows Device Manager. If properly connected you should see two USB Serial Devices. My computer chose com ports 5 and 7. Your computer may use a different number.
-
Next, make sure that all other programs that could connect to Arduino Opta have been closed. For example, close the traditional Arduino IDE, all terminal programs, or any scripts that you may have used to connect to Arduino projects in the past.
-
Launch the Arduino PLC IDE.
-
Open a new project. Give it a name and then ensure that the target selection is set for the Opta.
-
Open and expand this window until you see the red circled port selection options. Use the lower of the two port numbers as previously identified by the Windows Device Manager.
This article is part of the DigiKey Field Guide for Industrial Automation
Location: Program It → PLC → Arduino Opta
Difficulty:
Student — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 13 Mar 2026
-
Select Download.
-
Wait a few minutes for the software to compile and communicate with the PLC. Note that the IDE may appear frozen for a period of time.
-
When complete, you should green status indicators as shown in this picture.
- Click on the circled part in the above picture. If all goes well, you should see this in the lower right of your screen.
If you run into problems, please share your experience and solutions. Your assistance in refining this guide will be greatly appreciated by other.
Thank you on behalf of our readers.
Best Wishes,
APDahlen
Continue Exploring Industrial Control Systems
If this discussion was helpful, you may also want to explore:
DigiKey Navigation
- Full Catalog: Industrial Control & Automation
About This Author
Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.
Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.
Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.