I would like to know if open Mvcam H7 can be connected to Arduino board?

I would like to know if open Mv​cam H7 can be connected to Arduino board?

Hi tachapkarantee,

From reading a bit about it, it looks like the OpenMV Cam has multiple serial interfaces, including I2C, SPI, and UART, so it would be capable of interfacing with pretty much any Arduino platform via one or more of those serial protocols.

Here are a few of our OpenMV Cam options:

As an example of how one might do something with the Arduino/OpenMV Cam H7 combo, I came across a pretty nifty video showing how one can use them to implement a face-tracking application.

How do I order? Do I need to fill in the order form? What should I do if I don’t have these fields?Do I have other payment options such as cash on delivery?

ในวันที่ พฤ. 30 ต.ค. 2025 23:02 David_1528 via DigiKey TechForum - An Electronic Component and Engineering Solution Forum <notifications@digikey.discoursemail.com> เขียนว่า:

You can add the required quantity of each part to your cart directly from its product page. Please note that COD is not an available payment method. For more information, see –