Need specification and connection details of IMX490-GW5400-GMSL2-120H

Hi Team,

We have requirement for IMX490-GW5400-GMSL2-120H camera to connect to our Nvidia Jetson AGX Orin Industrial Box PC - DSBOX-AGX, You can find the our board details and specification from this link Jetson AGX Orin™ Industrial Box PC - DSBOX-AGX.

We gone through your site and found this camera specification LI-IMX490-GW5400-GMSL2-120H Leopard Imaging Inc. | Sensors, Transducers | DigiKey

Before We place the order, I want know the compatibility, connectivity process and it dependent cable required to connect to our Nvidia Jetson AGX Orin Industrial board.

Could you please help us on the above ask , if required let’s setup short call on for clarification to decide the final call.

Thank you for contacting DigiKey Technical Support and welcome to our community!
We are looking into your question.

The camera actually does not connect to USB as is currently in the product attributes, (An error report has been submitted for this). The connection from the camera is a FAKRA Z Type connector. For the setup that includes the camera and adapter the 2289-LI-USB30-IMX490-GW5400-GMSL2-120H-ND will need to be ordered for much greater compatibility with the ORIN.

Datasheet

The datasheet for the adapter notes that it has support for Windows, Linux OS and other OS which include the UVC drivers. If you can have UVC drivers in your ORIN unit, then you should be covered.

2 Likes

Hi Steven, So is this compatible with Orion board with given specification in the screenshot to connect the LI-USB30-IMX490-GW5400-GMSL2-120H camera with our Orin board . Is there any additional drivers required for this. Please confirm

I found this post regarding the UVC drivers and the ORIN.

As long as you are able to install the drivers, you should be able to use any camera with supports UVC drivers.