IDEC switch AS6-Y

Hello, I’m looking for the sitch in the picture
ON/OFF
AS6-Y frame
250V AC 0.5A
30VDC
IP65 TYPE
6 prongs

Hello,

Welcome to the TechForum !

I was able to locate a few similar options on this link here, 2 seem to be in stock currently.

Thank you

Ryan

Hi benoit.mercier,

I am not seeing that exact model within our inventory and I could not find data on your specific part number. However, I did find the AS6M-2Y2P, which seems likely to be somewhat similar.

However, without seeing the top side of your switch, I can’t say how close the two are to each other. From the datasheet, it looks like the image below and has a double pole double throw rotating selector switch which maintains its position (not spring return type):


Figure 1. Image of AS6M-2Y2P (page 8 of datasheet)

The specifications are not identical. This part is rated for 0.5A at 240Vac rather than 250Vac, and 1A only up to 24Vdc rather than 30Vdc. It is rated IP65 and the contacts appear to have the same arrangement, as seen here:


Figure 2. Image of contact configuration (page 11 of datasheet)

And physically, it would have the following dimensions:


Figure 3. Dimensions of AS6M-2Y2P (page 12 of datasheet)