Looking for this slide on/off switch

Hi there!!

Looking for this on/off switch with the same dimensions as in the link;

https://www.amazon.ca/gp/product/B00RVFHU82/ref=ewc_pr_img_1?smid=A24JGA3DO5B17D&psc=1

THANKS!!

Hello,
Welcome to the Digikey tech forum. This switch is listed with a rating of 3 amps at 250vac and we have no options to offer in that range. Do you need a 250vac rated switch? We have these similar options rated at 125vac. You’ll need to verify the voltage and dimensions to be sure one will work for you.

Hi I just need the 125v, 6+ amps but need the same dimensions;

  • 3.5 x 1.2 x 1.8cm/ 1.4" x 0.47" x 0.7" (LWH)
  • Pin Spacing : 5mm/ 0.2";Hole Diameter : 2.5mm/ 0.1"(Fit for M3 x 0.5 Size Screw)

Screen Shot 2024-03-12 at 4.35.39 PM

I need this EXACTLY as pictured.

THANKS!!! :grin:

Do you have a link to the data sheet?

It’s not @ the Amazon page and I couldn’t locate in a search.

The dimensions you have listed are not enough to ensure an exact match on all the dimensions

I don’t have a data sheet just this Amazon link to that part.

Ok did my own measurements with my digital caliper and this is what I have; 1.378" L x .497" W x .344 H
Screw holes at 1.136" (all measurements give or take .001-.002"). Here’s are pics of my part at home;

Hope it helps a bit.

Hello slebel,

The closest match I found is CWI328-ND.
Measurements are slightly different, but hopefully this one will work for you.
Please check the Datasheet, and the Drawing, for compatibility to your application.

There are too many unknown critical dimensions to be certain if any particular alternate part will fit well in that particular PCB and housing combination.

This includes:

  • Offset from the body centerline to the pins centerline
  • Spacing between mounting holes
  • Slide handle height and width

I’d just buy the exact part from Amazon, especially if you have free Prime shipping.