Identify a connector

I want to identify the connector in the image. It is for a FLIR Duo Pro thermal camera. Thanks for your help.

10-pin locking connector

a = 0.226 in deep

b = 0.535 in long

c = 0.075 in thick

Hi mckennat ,

Welcome to the TechForum.

The most important dimension you can give us is the pitch of the connector, which is the spacing from one contact to the next. Without this dimension, it’s very difficult to narrow down the options.

For small connectors like that, the best way to do so is to measure the distance from first to last contact, and then divide that distance by one less than the number of contacts, which in your case would be 9 (10 contacts minus 1). From there we can filter for 10-pin connectors with pitch values close to what you measured and go from there.

Here’s a starting point prior to filtering for pitch.

Hello mckennat,

Welcome to DigiKey TechForum.

A possible match is 455-1600-ND.

Please check the datasheet to verify compatibility.

1 Like

Thanks. That looks like the correct one.

I thought the metal inserts came with it. My bad. Is this the right part to order?