Black rectangular 10 pin connector

Hello,

I am trying to find this 10 pin rectangular connector. This is a crimp style

Size: 1.6mm x 0.9mm x 1.1mm (LxWxH)
The pins are 0.2mm apart
The connectors inside seem to be square shaped crimped.

Please see images on the below link:

Link: Imgur: The magic of the Internet

Please help

Welcome to the DigiKey TechForum shariqahmed321.
We are unable to open links from that website. You should post the picture directly on the post.
Also, we do not carry any crimp connector housing, that small, with a 0.2mm contact spacing.



I have uploaded the pictures here, hopefully this helps

Max upload is 3 images, I will upload last one separately

+1 upload

Hello,

Thank you for the pictures. Though I am in agreement with David. I do not see anything with the .2mm pitch. Sorry. I do not find anything.

To begin with, that is a 12pos connector, and not a 10pos. It may be close to 0.2cm (2mm), but is closer to 3mm. Let me do some searching.

Click here for 2-1827864-6-ND.
This looks close.
Click here for the available crimp contacts.

Thank you David!! Sorry, yes it was 12 pos - Thank you for the catch!

Thank you so much!