Identify terminal connector for ECU

I am looking for I believe a female terminal connector for a motorcycle ECU. Honda is the manufacturer. See attached photos



Thank you

We can’t identify contacts from photos. We would first have to identify the connector and then what contacts are used. Do you have a photo of the mating side of the connector? Are there any markings on the connector housing?

Hi, yes it’s for a motorcycle ECU harness of a 2022 Honda grom. Here is the connector block.



It is giving me “40 position 2 row card edge plug” vibes, but I couldn’t ID a part that fits the description and your photo.

Was there any other markings or info on the part?

It’s a 36 pin connector and the manufacturer is TE. Letters and numbers on it are PBT-GF15


Update: So I contacted TE connectivity since that’s who the manufacturer is. And they told me it’s a restricted part only sold to Honda. 2294140-2 20467 is the part number. That’s for metal contacts and connector housing.

Hello,

Since that is a proprietary part only sold to a specific manufacturer there isn’t much DigiKey can do in obtaining it nor the associated terminals for it. Sorry for the inconvenience.

Yep figured as much just thought I’d share an update to the ones who replied to this thread. Thanks anyway

I found an alternative terminal via contacting support at TE connectivity. They provided me this link https://www.te.com/en/product-1-2236793-3.html and I received samples of the terminal and they do work as a replacement for what I needed.