Interlock Switch SPDT Momentary on

I’m not entirely sure what the MFG for this specific momentary switch. It’s a momentary on SPDT 6A 30VDC. The closest thing i found was a Xerox 4110FDIS or 110E11980. I have photos of the switches markings. The manufacture is FUJISOKU I’m also looking for the datasheet as well.



Fujisoku appears to have been acquired by Nidec Copal, and I suspect that the CF-DD-2MZ0-K3 string is all or most of the part number.

Unfortunately, I’m not seeing that as an item of common trade. It’s not unheard of for mass-produced products to incorporate custom components that aren’t available off the retail shelf, and I’m not finding much at all that would come close as a possible replacement.

Hello TechMonkey:

I located the same information that Rick gave you, and did not find that part number available either. I did see one that looks like it may be comparable. This is also a Nidec option - here is the datasheet for this switch. (Nidec acquired FUJISOKU around 2007). You can compare the dimensions of this to your switch to see if you feel it could work as a substitute for the one you have, but these are SPST. We don’t stock this switch but we should be able to order this for you as a non-catalog order. Our non-catalog quote department would check with the manufacturer for lead time, minimum order quantity and pricing and get back to you with a quotation. It usually takes about 3-5 business days to receive a quotation. Unfortunately, I did not find a stocking alternative switch to offer you. If you feel you’d like to receive a quotation on the SPB101 switch, you can contact me via e-mail jenny.reigstad@digikey.com or contact our quote department quotes@digikey.com with the quantity you need and your full contact information. Shipping address, city, state, zip, phone number, etc,

One thing I would point out is that the internal schematic shown on the side of the switch would indicate a DPST (double pole single throw) rather than SPDT (single pole double throw).

image

Thanks everyone for the help, I think this is one of the first switches that I have come across like you all said isn’t available for resell. Thanks for all your time and help.