We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
Hello,
Welcome to the DigiKey TechForum. Typically, PMICs charge LiPo and Lithium-Ion batteries using the CC-CV method. The battery gets charged with a constant current until the cell reaches its maximum voltage. From then on, the charger gradually decreases the charge current until the battery is fully charged. Modern charge ICs apply a few more steps to the process to increase safety. These ICs monitor the cell temperature and have a programmable cut-out function that stops charging the cell after a pre-set period.
It has a maximum discharge current of 3.9 A, but a maximum charge current of 1.6 mA. This comes with several stipulations/cautions such charging at temperature extremes. There is also a cycle life that is specificized at significantly lower charge and discharge current when compared to maximums. The implication is that lower currents prolong battery life.