Is this capacitor a suitable replacement?

Hello!

I could use some help verifying if I’ve found a suitable replacement for a capacitor or not.

Here are two photos of the existing cap that’s not working.



Dimensions: 4.650"O.A.L., 3.710"L on can X 1.760"Ø w/ .30" stud and 4 spade, insert terminals @ .25". A replacement doesn’t have to be those exact dimensions, but should fit within them.

Would this part work?
CAP FILM 30UF 5% 450VAC RADIAL

If that part is an inappropriate choice, what should I use? Thanks in advance.

I would go with the 470VAC options. Here are any that will work as replacements.

Please review the datasheets and choose the one that best suits your application.