We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I purchased one of these to work as a thermostat inside a heated chamber. However in my test closure It does not turn the heater off when the temperature is well over 80° C according to the oven Thermostat that is in with it. I simply have this wired directly in line between the heater and the 120v power cord.
Thank you for contacting Digi-Key , this thermostat is only rated for 0.5A @ 140VAC , my best guess is that you have welded the contacts together by too much current . The first thing you need to know is what is the heating element current draw ? You may have to run this thermostat in line with a relay to turn the heater on and off . Something like this , part number 2449-J115F31A120VACS-ND , this is rated for 40A on the contacts .
The relay I offered before will work part number 2449-J115F31A120VACS-ND , but the data sheet that you have linked shows that they are using FTO 011 which is a thermostat , I have found 2 part numbers for that one which we do not have Those part numbers are 01160.0-01 and 01160.0-00 , I did find some at a place called Galco they have them in stock , https://www.galco.com , Data sheet https://www.galco.com/techdoc/stgo/01160.0-00_dat.pdf
Thank you for your quick and helpful replies. I need a thermostat that cuts off at 80 degrees Celsius… Preferably I would like a variable one that goes that high, but I haven’t found one. Any that fit?