Kyocera TCTOBL1E156M8R-ZB1 msl3 shelf life and rebake

Kyocera TCTOBL1E156M8R-ZB1 msl3 shelf life and rebake
Hi - our factory has some old - date code 2022 - tantalum caps.
in original sealed packaging.
and from what I see on the datasheet they are moisture sensitivity level 3

I am trying to find out the recommended shelf life and if these parts can be re-baked and used.
or if that is not recommended by the manufacturer.

Any help appreciated
Craig Stapleton

Hello, welcome to the TechForum!

I checked the manufacturers website for more information on this part, but unfortunately I was unable to find any additional resources for baking this part. I believe since it is still in its original packaging, and if the humidity indicator card shows that no moisture leaked inside it, then the part should still be usable.

1 Like

Component “shelf life” might be one of the more widely misunderstood topics in the industry.

The main question there is solderability: protracted exposure increases the amount of oxides/sulfides/schmoo that forms on the component terminals, potentially impeding the reliable formation of a solder bond.

But said schmoo begins forming immediately upon manufacture however, and is present on pretty much every component regardless of age; that’s why solder flux is a thing. The rate at which schmoo forms is affected by storage conditions, and the amount of schmoo buildup necessary to cause solder joint failure at some specified defect rate is affected by the solder process and materials used: all such things are outside the manufacturer’s knowledge or control.

Folks don’t like indeterminate answers of that sort and like accepting responsibility even less, so some manufacturers throw out a very conservative and conveniently-round number as a “shelf life” figure that’s likely to give acceptable solderability for most storage conditions short of a continuous saltwater mist… The problem with doing so is that it results in a lot of perfectly serviceable parts being wasted and creates a nasty logistics/supply chain issue.

if these parts can be re-baked and used

The blunt answer is that they’re your parts at this point: whether you choose to use them in the typical fashion, add them to your granola for extra texture, or mix them with legos and sprinkle them across the bedroom floor is completely and totally up to you. However, all responsibility for the results of those choices is also yours.

This post has some useful references.