Hello.
I am builing a project that simplified is a dolly moving on a track.
When the dolly reaches the end of the track, it triggers a microswitch that cuts the power to the motor, and redirects the power to a LED to light up to indicate that the switch has been triggered.
My problem is that since the motor controller I am using changes the polarity of the motor to make it go left or right, I am getting positive and negative voltage every other time. (depending on if the dolly is moving right or left).
I have tried to use a 12V relay to trigger and light the LED, but the problem with that is that the relay needs at least 6 volts to latch, and when the motor is running slow, the motor controller only provides 3-4 volts.
Is there anyone that has a sollution on how I can make this work? I am just starting to fiddle with electronics, and I am on a bugdet with this build, so therefore: Is there a relatively easy fix for this problem? Are there relays out there that has a latch range from 3V to 12V?
Attatched is:
1: Schematics of the circuit with the LED (and resistor) connected directly to the microswitch. The problem here is that every other time the positive and negative switches.
2: Schematics of the circuit with a relay attatched to the 2nd output of the microswitch. The problem here is that the relay need 6 volts to latch, and the motor controller doesnt provide that at slow speeds.