I am looking for a part number for the power cord for a GE Panametrics PT878. I know it is a Lemo Circular Connector and it is 4 pin. The power supply itself is 12v 3.3A so that is not an issue. I am looking for a part number and availability?
Welcome to the community!
I couldn’t locate a 4-position half-moon connector like that in our system. I also don’t see a cable in our system with that end. Where did you purchase the unit from?
Looks like you have an ECP Model Lemo Connector
Determining the series size you’d need to figure out what e thread is in the below dimensional diagram. Maybe M12x1.0 thread which would be the 1S series.
Possibly ECP.1S.304.CLL from LEMO double check the dimensions against the above drawing.
A=12mm
e=7mm about I am not sure if that relates to M9x0.6
If it does end up being the 0S series here is an option I’m seeing for mating connector that accepts a cable opening of 0.146" ~ 0.173" (3.70mm ~ 4.40mm)
FFA.0S.304.CLAC44 LEMO | Connectors, Interconnects | DigiKey
I will give it a try. Thank You.