Littelfuse component compatability for FH2/FKH series

I just had a few compatibility questions for the Littlefuse sets from their datasheets:

  • Do all the 178.6116.2501 / 178.6116.1001 / 178.6116.6001 Littlefuse terminal contacts fit into both 178.6150.0001 and 868-900-010RM housings?
  • Can the 178.6116.2501 terminal contacts be crimped with the Japanese Hozan p-707 crimper, or is there another crimper that’s better suited within the same price range?
  • Does the 178.6152.0001 come with the 178.6116.1001 (0.5-1.0mm²), the 178.6116.2501 (1.5-2.5mm²), or the 178.6116.6001 (4.0-6.0mm²) contacts?

The datasheets is have don’t seem to confirm concretely:

https://www.littelfuse.com/assetdocs/ato-fkh-datasheet?assetguid=52ab370f-f59e-4f6c-87fb-d18075289d4c

https://www.littelfuse.com/assetdocs/ato-fh2-datasheet?assetguid=2cfefd9b-6d4e-4228-b3c6-09e63cb830b8

Posting here as suggested by a Digikey rep, and in case someone else had the same question. I may reach out to Littlefuse themselves, so I’ll post back with their thoughts if they have any answers.

Thanks for any help,

Hi @CKDW

Here is what I found in the Littelfuse documentation:

  1. Housing: These contacts are listed as FH2 parts, so I’d use the FH2 housing (178.6115.0001). They will likely fit the FKH housings too, but Littelfuse doesn’t confirm it.

  2. Crimping: Littelfuse doesn’t name a recommended crimp tool.

  3. 178.6152.0001: It comes with its own DFK-2 spring leaf terminals (Littelfuse part 376.1414.2225), not the 178.6116.x contacts.

That being said, I’ve contacted Littelfuse about the FKH fit and the crimp tool, and I’ll update this thread when I hear back, if you haven’t heard from them by then.

Hi @CKDW,

Littelfuse got back to me with answers:

  1. Housing: The 178.6116.1001, 178.6116.2501 and 178.6116.6001 contacts do not fit the 178.6150.0001 or 868-900-010RM housings, so the FH2 housing (178.6115.0001) is the one to use.

  2. Crimping: The 178.6116.2501 is made by Lear (Lear part 26472.331.179), and no specific tool is listed for it and Littelfuse advised contacting Lear.

    I would recommend an open barrel crimper that accommodates 16-14 AWG (1.5-2.5 mm²) wire.

  3. 178.6152.0001: Its included 376.1414.2225 terminals accept 1.5-2.5 mm² wire.

Thanks @jon_11475 , this is all very helpful!

Also, I just noticed that the housing with the transparent lid (178.6105.1002) is double the price of both pieces (178.6125.0001 & 178.6115.0001) purchased separately, but I’m unsure if that is intended. This was for the Canadian site.

Hello @CKDW,

I can’t speak to exactly how they set the price, but the difference is likely intended, since the 178.6105.1002 includes the terminals, housing, and cover, per page 1 of the FH2 datasheet.

Best regards!