Looking for 16awg, 12-15A rated wire to board connectors

I have two power wires running between boards currently connected using a terminal block (Wago 2060-452/998-404) on each board. I am looking to replace these with some locking connectors rated for 16awg wire and 12-15A. One connector needs to be vertical and one needs to be right angle.

I’ve identified the Hirose DF63 connectors as a great option (vertical: DF63M-2P-3.96DSA; right angle: DF63M-2P-3.96DS), but the right angle connector is too large to fit in the constraints of my PCB board stack. I need a connector very similar to that that is no more than 8mm proud from PCB to the “top” of the connector. The vertical DF63 connector I listed works great and fits in the space provided at the opposite end of that connection, but I would like both connectors to be consistent for crimp contacts/manufacturability.

One additional note: It would be ideal to have surface mount connectors here. The Hirose DF63 connectors are through-hole which would work but is less than ideal.

Hello Braden,
Thank you for contacting DigiKey Technical Support.
These are the right angle connector options I was able to find for that pitch.

I am sorry to inform you that we do not have any surface mount options.