Part Identification

Looking for replacement low voltage connector. Was able to find “HRS” on the connector, but cannot identify anything else beyond that. Looking to purchase connector and female pins. Would also like to know what type of crimpers are needed as well.

See attached photos.

Thanks for reading, Brian



brianpacchetti

Thank you for contacting DigiKey , from what I am seeing it looks like this is part number H2083-ND But without knowing the pitch of the contacts I cannot be 100% certain , check data sheets to see if the dimensions are correct https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/827/DF3.pdf , there are several contacts listed for this housing in this link , Rectangular Connector Contacts | Rectangular Connectors | Electronic Components Distributor DigiKey

22AWG contacts use crimp tool H4454-ND and the 24 to 28AWG contacts use crimp tool H9997-ND

Thaks Craig

Hi brianpacchetti,

Assuming you have verified that the connector you are seeking is the DF3 type that @Craig_2048 has identified, you may have noticed that the specified crimp tools are not exactly meant for those on a tight budget. We do sell some jumpers with the contacts already crimped onto the wires which come in various colors, lengths, and permutations of contact types (female to female, female to stripped wire, female to pin, etc.) which may help to reduce your total cost significantly.