Looking for a cable part number

Hi, I’m looking for a particular cable, but I don’t know how to search for it given the information that I have. I’m working from a guide, which describes the cable as “FD female-to-female FD(1.27mm->2.54mm) winding displacement wire 2*8P;”. The picture in the guide is attached here.

It doesn’t necessarily need to be female to female; I can work with whatever header configuration that is handy. I need it to be short; or even a plug from the smaller size to the longer size. Thank you for any information you can give me.

Hello Bob,
Thank you for posting on our forum and welcome to our community.
The specifications I can see from picture.
2 row, 16 position, socket to socket.
These are cables we do carry with those specs.

The specs I cannot see is row space and pitch. I recommend using a micrometer to measure the pitch.

Hi, Thanks for the reply.

I have this cable now: FFMD-08-T-02.00-01-N
Here’s a link to the page.

This cable plugs into the socket I’m working with properly. What I’m looking for is something to convert this into a larger plug on the other end. I want to be able to plug wires into it to interface with a breadboard project I’m working on. The holes in the cable I have are too small to access easily.

I’ve used the page that you sent me, but there doesn’t seem to be away to specify that I want different sizes on the two sides. I may be misunderstanding how to use the page.

Thanks very much,

Bob