Looking for a longer cable similar as the HQCD-030-02.00-SEU-TBR-1

Hi team,
I am wondering if the cable HQCD-030-02.00-SEU-TBR-1 has a longer version?

The HQCD-030-02.00-SEU-TBR-1 is about 5cm long, and I am looking for a longer one like up to 10cm.

I found there were 2 possible options, HQCD-030-06.00-TEU-SEU-1 or HQCD-030-12.00-TEU-SEU-1 available, but I am not sure if these 2 are working the same as the HQCD-030-02.00-SEU-TBR-1?

Many thanks.

Hello @zyzzoo,

Welcome to the TechForum Community. The difference between the two options is the length, HQCD-030-06.00-TTR-STR-1 (0.500’ (152.40mm, 6.00" Length) and HQCD-030-12.00-TEU-SEU-1 (
1.00’ (304.80mm) Length).

To get this cable with the 10cm length, we would have to do a special quote on the part number HQCD-030-03.94-SEU-TBR-1. It is typically 3-5 business days for the quote. Please send me a private message with your customer number and quantity if you would like a quote.

Thanks!

2 Likes

Hi @Jeff_Aberle Jeff,
Thanks for your information. So, are these two options designed for working the same as the HQCD-030-02.00-SEU-TBR-1?
If so, I think the 15cm one HQCD-030-06.00-TTR-STR-1 should be good for my case. Or you may have to double-check if they work as the same by a special quote?

I am on one of my research projects, and I may just need 2 for research testing purposes.

Sorry for my mistake on the correct cable part numbers. We would have to special order HQCD-030-03.94-SEU-TBR-1 to get the correct cable with the same connectors and length. Send me a private message with your customer number and quantity so we can start the quote.

Thanks!

1 Like

@Jeff_2258 I see, so these two may not work the same as the HQCD-030-03.94-SEU-TBR-1.

So, I am wondering how could I send you a private message?

Just click on my user name to be able to send the message.
image

@Jeff_2258

It seems there is no message button when clicking your user name. So, can you please message me and then I reply? Thanks.

Just sent you a PM.

1 Like