Looking for a connector in the image. 4 pin connector Thanks
Hello Speedcrew,
We need more information to search for a possible match.
What is the pin spacing (pitch)? What do the mating pins look like? What does the opening for the mating connector look like? Are there any board guides that stick through the board, under the connector? Do you have a picture of the mating connector? Are there any markings on this connector?
Just looking for something that looks similar, Click here for 455-S4B-ZR-SM4A-TFCT-ND.
You can check the datasheet, and compare this connector with the answers to the above questions.
Hi David, no markings.
Pitch is .91 mm.
Here is a picture of the connector that goes to it.
Thanks
Mating pins in this one
That logo is Hirose.
Kindly see below:

DF13A-4P-1.25H(51) Hirose Electric Co Ltd | Connectors, Interconnects | DigiKey
DF13-4S-1.25C Hirose Electric Co Ltd | Connectors, Interconnects | DigiKey
Thanks for the added information Speedcrew.
The HRS is the symbol for Hirose Electric Co. I seem to find a close one, which is 26-DF13-4P-1.25H(51)CT-ND, but this one has a pin spacing of 1.25mm. So the width of the connector, not including the tabs on the sides, is 6.65mm +/- 0.2mm. The mating connector is H2181-ND.
I’m sorry, but we do not have a match to the 0.91mm pitch.