I’m looking for this plug. Do I need to measure anything? I have some plugs that are 2.8mm but are too large. I will need the housing and pins for both male and female.
Hello @bjec607,
What is the pitch (center-to-center) spacing from pin to pin? Are there any markings on the part? Can you provide a few more photos?
Hi @bjec607
Based on your photos, this looks like the JST YL series, a 4.5mm pitch connector. Please confirm the dimensions prior to order.
YLP-06V, DigiKey part number 455-3760-ND
YLR-06V, DigiKey part number 455-3787-ND
6 pin, not 9. looks more like the JST. My question is pitch is closer to 4mm, or 3.9mm, not the 4,4 or 4.5mm. Does the JST make a 3.9mm pitch?
Ron
I just went and measured the overall width and thickness. The plug is 4.8 x 2.6 overall.
wrong. 14.8 x 12.6mm. Sorry
It appears that more than one connector has been pictured above. Which one is the topic of discussion?
Pitch measurements made by eyeballing contact centers tend to be quite inaccurate, and one should account for that fact when trying to make an identification. The suggestions above appear to be quite good.