Mates to D38999/23YA35PN & D38999/23YA98PA

We are using D38999/23YA35PN (6pin male) and D38999/23YA98PA (3pin male) circular connectors to penetrate a pressure vessel wall. I am looking for the mating connectors that would be connected on the non-pressure sensitive side including any backshell and strain relief required for the cables.

Also any hand crimp tooling that may be required for the mating connector if the wire termination on the connector isn’t a solder cup.

Hello, Welcome to the TechForum!

I was able to find parts 1178-D38999/26FA35SN-ND and 1178-D38999/26KA98SN-ND as the mating connectors for your parts, and 952-1238-ND as the crimp tool for the contacts.

As we do not need the hermitic sealing on the mating connector, is there something in their catalog that will mate?