Hello artvandalai, and welcome to the DigiKey TechForum.
Using the Resistor Color Code Calculator, it does appear that this is a 47ohm 0.1% resistor.
I wasn’t able to find any information stating for certain if this was fusible or flame retardant, but we do have a couple 47ohm 0.1% resistors, linked HERE. One is listed as Flame Retardant but is also only 1/8W and the other is listed as 1W.
Based on some information I was able to find online, there was conflicting possibilities for the wattage, one stating 1/2W and another stating 1 or 2W. I was also unable to find a service manual that mentioned a replacement Resistor. Of the two linked above, MMFR6518B47R0V9, is more likely to possibly work but I could find no information to confirm this.
As a note, the two above linked resistors are the only normally stocking and active 47ohm 0.1% resistors I see listed on the DigiKey website.