I need part numbers for a 12 inch and 36 inch ribbon cable as shown in image attached.
It says Bando AWM 20624 VW-1 Either this exact Mfr. or a similar cable from another Mfr.
This cable is 1inch wide and 27 conductor
Hello,
Welcome to the DigiKey TechForum. I did some searching and wasn’t able to find any options to offer for these two cable lengths that match the width of your cable.
andrewtjason
Thank you for contacting DigiKey , sorry I am not seeing that we have a 36 inch one to offer , for the 12 inch take a look at part numbers 0152670985-ND or 0151670985-ND these are 1mm pitch so the total cable width is 1.1 inches and they both have contacts Top on Both Sides, Backers on Both Sides . Check data sheets to see if either will work for you .
Thanks Craig**
Thank you so much! Did you find any lengths larger than 1 foot? 2, 3, 4, or even 5 feet or larger?
If not can you suggest another manufacturer or supplier? Thanks again.
Hello Again:
I answered your email before I saw your other email with the suggested part numbers. I think they will work for me. I will order and find out.
Thanks again.