I’m trying to replace a ribbon cable: 1.0 Pitch 16 Pin 550mm Flexible Flat Cable CHS E248204 AWM 20624 80C 60V VW-1 (See link for photos)
The issue is I have no idea how to find this.
Hi NoJimCarrey,
Welcome to the community!
If we had these they would fall under the category Cable Assemblies > Flat Flex Ribbon Jumpers, Cables
The only thing missing in your description is if the conductor contact ends are facing the same side on the cable or opposite sides.
You’re going to find the longest option we have available, in stock in 16 conductor, 1mm pitch (spacing) is length: 18.0" (457.2mm) which would have top (contacts) on same side.