Need reference

Hi, i need cross reference for this part (varistor ?)

thanks

Hello rep-levis, thank you for the question! It could be a varistor or it could be an inrush current limiter. Is it a 20mm disc with a green coloring? The picture is a little hard to tell the exact color.

Diameter is 20mm, color is grey

Valiue ohms

Best regard

I think it could be one of these obsolete ICL’s: click here.

The closest stocking alternate we have is 4378-MF202R508M1DN0CSB0-ND which has the same diameter or 317-1208-ND.

Hi rep-levis,

I suspect @Kaleb_Kohlhase is onto it as an inrush current limiter (a special type of NTC thermistor). I found this datasheet, which seems about right.

Based on that datasheet, it’s a 12Ohm @25°C, 5A, 20mm diameter part.

These options seem to be in the ballpark, with the following as probably a decent choice:

CL-60 10 Ohms @ 25°C, 5A, 19.5mm diameter

David you’r right, i mesure, the value is 11.7ohms.

it’s inrush Current Limiter.

many thanks guy