Can anyone help in identifying Part value for varistor 125 006?

Take a look at this post.

Unfortunately, they did not reply to see if it was the same part.
-Robert

Based on this answer and my research, part number : SL32 0R540 is making more sense to be close match. According to the Datasheet of SL32 0R540 dimensions (30MM diameter and ~5mm thickness) are exactly the same as 125 006. Plus, the resistance value for both are matching too.

again this might be wrong but I will keep update as find more information and practical experiment.

thank you